Introduction to Boost Converter Circuit

Boost Converters (DC-DC Step-Up) - Electronics Intermediate 1
I. Working Principle
It is mandatory that you know how inductors, MOSFETs, diodes, and capacitors function in order to understand the operation of a boost converter.
With that experience, step by step, we can go through the operation of the boost converter.
Phase 1:

Nothing occurs here. Minus one diode drop, the output capacitor is charged to the input voltage.
Phase 2:
It's time, now, to turn on the light. The source of our signal goes big, turning on the MOSFET. All the current is redirected via the inductor to the MOSFET. Remember that the output capacitor remains charged as the now back-biased diode does not discharge into it.
The power supply is not short-circuited instantly, Of course, as the inductor relatively slowly makes the current ramp-up. A magnetic field also accumulates around the inductor. Notice the voltage polarity that is applied through the inductor.
Phrase 3:
The MOSFET is switched off and the current is suddenly halted by the inductor. Maintaining steady current flow is the very essence of an inductor; it doesn't like abrupt current shifts. So the abrupt turning off of the current doesn't like it. It responds to this by producing a large voltage using the energy stored in the magnetic field with the opposite polarity of the voltage originally supplied to it to sustain the current flow.
If we ignore the rest of the circuit elements and consider only the symbols of polarity, we notice that the inductor now behaves in series with the supply voltage like a voltage source. This implies that the diode anode is now at a higher voltage than the cathode (remember, at the beginning, the cap was already charged to supply voltage) and is biased forward. The output capacitor is now charged to a higher voltage than before, meaning we have increased a low DC voltage to a higher one successfully.
II. Selection of the Right Boost Regulator ICs
We've all come across circumstances when designing electronic circuits where there is a need for a slightly higher voltage than can be given by the power supply. There is also a need for 12V from a 9V battery, or maybe 5V from a 3.7V lithium battery is needed for your application.
The solution is often referred to as a boost converter, which can transform DC low voltage to DC high voltage. It takes an input voltage and boosts or lifts it, as the name implies. It consists of an inductor, a switch (a MOSFET, probably), a diode, and a capacitor. A switching square wave that we can provide with a function generator or a 555 timer IC is also needed.
There is a Synchronous Boost Converter to improve the performance of the boost converter, in which the circuit construction remains the same, but the diode is replaced by a MOSFET to decrease the loss. So, let's make this article an opportunity to find out other than the iconic MCP16252, NCP3064, MC34063A, etc., some of the smallest, cheapest, and widely used boost regulator ICs available on the market If you want to try other regulators other than boost regulators, you can also find out how to pick the linear regulator IC.
1. HT7733 by HOLTEK 100mA
The HT7733 has an input voltage range of 0.7V - 0.9V and is a very modern, low-cost, single-chip, step-up (boost) regulator. This IC is made for modern-day lightweight apps with many kit choices.
This IC only comes with fixed voltage versions, so it is not possible to change the output voltage, it comes with a 100mA maximum current rating, so it is used for compact applications with low power. For different voltage choices, please refer to the datasheet on this IC. This IC has a 115KHz fixed switching frequency. This IC can achieve an efficiency of 80 percent with this (assuming limited load condition).
Other Features: Pulse frequency modulation (PFM) based driver circuit for low noise operation, Ultra-low supply current of 4uA, Low ripple and low noise, Low shutdown current: 0.5A & more.
Protection Features: Under-Voltage Lockout Protection, & Over-Temperature Protection.
Applications: PDA Driver, Portable communicators, Cameras, Battery-powered equipment & more.
2. TPS610992 by Texas Instruments
A very modern, low-cost, single-chip, synchronous step-up (boost) regulator with an input voltage range of 0.7V to 5.5V is the TPS610992. This IC is made for ultra-compact applications with a 1.23 mm x 0.88 mm WCSP(6) kit.
This IC's output voltage can be set to anywhere from 1.8V - 5.5V. This regulator can withstand currents up to 800mA continuously with a 0.25 ⁇ internal control MOSFET. For more information, please see the datasheet of this IC.
This IC has a 120KHz fixed switching frequency. This IC can achieve an efficiency of 95 percent with this (assuming light load condition). The efficiency drops to 74 percent with a maximum load of 800mA.
Other Features: True Disconnection During Shutdown Mode, 1-µa Quiescent Current Under Light Load Condition, Additional Down Mode, and Pass-Through operations for different applications & more.
Protection Features: over-temperature protection & Over Voltage Protection.
Applications: Memory LCD Bias, Optical Heart Rate Monitor LED Bias, Wearable Applications, Battery-Powered Systems & portable products.
3. SE3608 by Allegro Seaward Electronics
The ME2188 is a rather modern, low-cost, single-chip, step-up (boost) controller with a 2.5V - 6V input voltage range. This IC is made for modern-day lightweight apps with a SOP8 kit.
It is possible to change the output voltage of this IC to anywhere between 2.5 - 10V. This regulator will manage the output current of 2A continuously with a 70-m or 0.007-internal power MOSFET. For more information, please see the datasheet of this IC.
This IC has a 1.2MHz fixed switching frequency. This IC will achieve an efficiency of 93 percent with this (assuming limited load condition). The performance drops down to 85 percent with a maximum load of 2A.
Other Features: Internal Soft Start, 1uA Shutdown Current, Accurate Reference: 0.6V VREF & more.
Protection Features: Under-Voltage Lockout Protection, Over-Temperature Protection & Internal Soft Start.
Applications: A power source for battery-powered equipment, Li-Po Charger, Digital Cameras & Portable Products.
4. MC34167 by ON Semiconductor
A very modern, low-cost, single-chip, the configurable voltage regulator is the MC34167, which means it can be programmed as a configuration for the buck, boost, or invert. With a TO220 & D2PAK kit, this IC is made for high-power applications with an input voltage range of 2.5V - 40V.
This IC's output voltage can be set to anywhere from 1.5 - VIN. This regulator can accommodate an output current of 5A continuously with a 0.08-internal control MOSFET. For more information, please see the datasheet of this IC.
This IC has a 72 kHz fixed switching frequency. This IC will achieve an efficiency of 85 percent with this (assuming limited load condition). The performance drops down to 65 percent with a maximum load of 5A.
Other Features: Internal Resistor for Fixed %V Output, Precision 2% Reference, 0% to 95% Output Duty Cycle, & 36uA Current Draw at Standby Mode.
Protection Features: Under-Voltage Lockout with Hysteresis, Cycle−by−Cycle Current Limiting & Internal Thermal Shutdown Protection.
Applications: A power source for battery-powered equipment, Li-Po Charger, Digital Cameras & High-Power Applications.
5. LT8471 by Linear Technology
A very new, single-chip, synchronous boost regulator with an input voltage range of 2.6V - 50V is the LT8471. This IC is produced for very dual power applications with a 20-Lead TSSOP and 28-Lead QFN Kit.
It has two output channels, one can handle a maximum current of 2A, and the other can handle a maximum current of 500mA, as this is a special type of IC. A buck, boost, sepic, zeta, flyback, or dc/dc inverting converter may be the 2A primary channels. The 500mA skyhook channel produces boosted input voltage efficiently. The output channel voltage can be changed to between 4.5V and 50V for both.
The switching frequency of this IC can be changed to 1.55MHz - 2.0 MHz. It can achieve an efficiency of 95 percent with this (assuming limited load condition). The performance drops down to 75 percent with a maximum load of 2A.
Other Features: UVLO and OVLO Programmable on OV/UV Pin, Soft-Start Programmable for Each Channel, Fixed Frequency PWM (Set by RT Pin or Synchronized to External Clock), Anti-Phase Switching Reduces Input Ripple
Protection Features: Output Overvoltage Protection, Cycle-by-Cycle Overcurrent Protection, Thermal Shutdown & more.
Applications: Dual Rail Power for Signal Chain & Buck/Buck, Buck/Boost, Boost/Boost, Boost/Invert, Invert/Invert, Buck/Invert.
Does boost converter increase power?
So we store some energy in the inductor from the input and transfer that same energy to the output though at a higher voltage (power is conserved, obviously). ... However, since energy is proportional to the square of the maximum current, increasing the current will lead to a larger increase in output energy.
How do I create a boost converter?
In a boost converter, the output voltage is greater than the input voltage – hence the name “boost”. A boost converter using a power MOSFET is shown below. Here VD is the voltage drop across the diode Dm, and VTrans is the voltage drop across the transistor M1. The inductor shown in Fig.
What is the difference between buck and boost converter?
In PV applications, generally, a Buck converter is used to charge the battery (since the output from a Buck converter is supposed to be less than its input), while a Boost converter is used to "match the load voltage" from the (supposedly) low voltage PV input.
Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap DevicesSaumitra Jagdale15 March 20242931For a long era, silicon has stood out as the primary material for fabricating electronic devices due to its affordability, moderate efficiency, and performance capabilities. Despite its widespread use, silicon faces several limitations that render it unsuitable for applications involving high power and elevated temperatures. As technological advancements continue and the industry demands enhanced efficiency from devices, these limitations become increasingly vivid. In the quest for electronic devices that are more potent, efficient, and compact, wide bandgap materials are emerging as a dominant player. Their superiority over silicon in crucial aspects such as efficiency, higher junction temperatures, power density, thinner drift regions, and faster switching speeds positions them as the preferred materials for the future of power electronics.
Read More
Applications of FPGAs in Artificial Intelligence: A Comprehensive GuideUTMEL29 August 20255745This comprehensive guide explores FPGAs as powerful AI accelerators that offer distinct advantages over traditional GPUs and CPUs. FPGAs provide reconfigurable hardware that can be customized for specific AI workloads, delivering superior energy efficiency, ultra-low latency, and deterministic performance—particularly valuable for edge AI applications. While GPUs excel at parallel processing for training, FPGAs shine in inference tasks through their adaptability and power optimization. The document covers practical implementation challenges, including development complexity and resource constraints, while highlighting solutions like High-Level Synthesis tools and vendor-specific AI development suites from Intel and AMD/Xilinx. Real-world applications span telecommunications, healthcare, autonomous vehicles, and financial services, demonstrating FPGAs' versatility in mission-critical systems requiring real-time processing and minimal power consumption.
Read More
The 2026 Engineer’s Guide: Choosing the Right MCU for Your Next IoT & New Energy ProjectUTMEL30 April 20262172A comprehensive comparison of 2026's leading MCUs from ST, NXP, and Microchip across power efficiency, processing performance, connectivity, and ecosystems to help engineers select the optimal chip for next-gen IoT and new energy projects.
Read More
AI Server Components: Engineering Next-Gen Data Center Hardware for 100kW RacksUTMEL15 May 20261146The transition from traditional enterprise IT to AI-driven workloads has rendered legacy data center hardware obsolete, forcing infrastructure planners to re-engineer server components for extreme thermal environments.
Read More
The Practical Engineer’s Guide to the NE555N Timer: Pinout, Setup, and TroubleshootingUTMEL29 May 20261000This comprehensive guide explores the NE555N timer, detailing its 8-pin layout, internal architecture, and key datasheet specifications. It compares the bipolar IC to CMOS variants and details setup configurations for astable, monostable, and bistable modes. Additionally, the guide offers practical troubleshooting advice to prevent common breadboard failures, such as floating reset pins and electrical noise issues.
Read More
Subscribe to Utmel !
KSZ8993MLMicrochip Technology
AT88SC0404CA-SH-TMicrochip Technology
ATECC508A-MAHDA-TMicrochip Technology
ATECC608A-SSHDA-TMicrochip Technology
HCS500-I/SMMicrochip Technology
AT88SC0404CA-SHMicrochip Technology
FSSD06BQXON Semiconductor
AD5522JSVDZAnalog Devices Inc.
HCS515-I/SLMicrochip Technology
AT88SC0104CA-SH-TMicrochip Technology


Product
Brand
Articles
Tools